I am currently working on a design using the 74LVC14A.
There is a condition that may apply a voltage greater than the supply rails to the output of the device through a resistor.
The datasheet for the 74LVC14A shows an output clamp current of -50 ma when Vo<0.
There is no mention of conditions where the Vo may be greater than VCC.
Is there a method to protect the output stage for a fault condition that may pull the output greater than Vcc?
Some of our previous designs used the 74ACT14 which has a output clamp current of +/- 20 ma.
This current rating was used to determine the value of current limit resistor.