Other Parts Discussed in Thread: TXS0108E, SN74AVC8T245
Greetings,
I´m using an TXS0108E Voltage level translator in the following app:
VccA=2.8V
VccB=3.3V
Max Speed= 115 KBPS
I employ it to interface a 2.8V Logic output UART to a 3.3V USB to SERIAL converter
The driver´s output maximum Load is 1mA at 2.8V, I was told that the auto sensing, bi-directional Voltage Level Translators usually have a
higher driver current demand that Uni-Directional VLT´S.
Is it OK to interface the TXS0108 with a driver with so low current capability?