Other Parts Discussed in Thread: TXS0108E, TXB0108, SN74LVC8T245
Hi,
Im using TXB0108PWRG4 to translate 3.3V input signal from FPGA chip to 5V output. The 5V input is used to drive a off the shelf power amp's control signal.
I realised that the output voltage drop from 5V to 1.8V when connected to the power amp. I believe this might be cause by the internal pull up / pull down resistor in the power amp.
Is there any recommendation to solve the issue? Is the any chip I can use to replace TXB0108PWRG4 with similar pin layout and size as my PCB board have been fabricated.