Other Parts Discussed in Thread: TXB0104, TXS0108E, TXS0102
I'm working on a design involving processors at different voltage levels.
1. I need to interface a uSD card with an Atmel ATMega328. Is the TXB0104 a suitable and correct device for such an application ?
2. I need to set up bi-directional communication between a Broadcom BCM2835 processor at 3.3V and the ATMega328 at 5.0V. The communication lines required are :
a. Two wire I2C channel (SDA and SCL)
b. Serial UART channel (Rx and Tx)
c. Two Spare signals from BCM2835 GPIO to the ATMega 328 (to be used, for example, for resetting the ATMega328).
For this, which device family is suitable - TXS or TXB ? You design guide indicates that the TXS series is suitable for I2C applications. Will the same type of device be suitable for Serial UART communications too ? If so, Can I use a single 6 channel device (for #2 a,b,c above) ?
Anool J M