Hi
Im using a TXB0104 for level translating on a debug port, A side is 1,8V and B side is 3,3V. OE is always connected to 1,8V for enable.
I dont have any pullup or pull down resistors on A or B side. Baud is 115 Kbps.
The problem is: I only get garbage on my terminal connected on the B side. When i connect a 1nF capacitor to A1 witch is TX from CPU to port A then
everything works perfectly, why does this happen ?
Signals on A1 is high in not used state and witout capacitor, when signals starte to flow i only get garbage on the terminal. drive strengt from CPU is set to high.
BR
Christian