Other Parts Discussed in Thread: SN74LVC1T45-EP, SN74AHCT1G125
Hello, I am going to use LVC125 inputs driven by the 3v3-powered signal, and its output should be +5v CMOS compliant.
I see from datasheet that I can power LVC125 from +5v. However with +5v power supply VIH voltage is defined as 0.7*VCC, which is 0.7*5=3.5V!
Will then 3.3v or below (let's say, standard TTL level when logical 1 is reliably recognized when input voltage is above 2.3V) be recognized as logical 1?
Thank you!