Other Parts Discussed in Thread: SN74AVC4T774
Hello,
Is it ok to pullup the DIRx and OE# pins to VCCB on the SN74AVC4T774 during partial powerdown? In my application, VCCA is 1.8V and VCCB is 3.3V and during partial powerdown VCCA is 0V. Currently the DIRx and OE# pins are tied to VCCA since they are powered by it. However, during partial powerdown, 3mA is drawn on the VCCB rail. Should the DIRx and OE#, be pulled up to VCCB in this case although they are powered by VCCA to minimize current draw? The 4T774 webpage references scea030a.pdf which indicates that this is ok (similar but different device) even though they are powered by VCCA.
Thanks.