Dear all,
Does the MAX Vin specified for sn74lvc08 (5.5V) applies only when VCC= 5.5V or within the whole range of VCC.
Thanks in advance.
Nuba
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all,
Does the MAX Vin specified for sn74lvc08 (5.5V) applies only when VCC= 5.5V or within the whole range of VCC.
Thanks in advance.
Nuba
Hi,
this part is LVC and no little logic, hence you must not apply a VCC of greater 3.6 V. (datasheet: operates from 1.65 V to 3.6 V). But the inputs are alway, independent of VCC 5 V tolerant (datasheet: inputs accept voltages to 5.5 V).
Regards,
Edwin Krasser
Yes, it can. The input can go to 5V even if Vcc is zero. Check the Ioff feature.
Thanks. Would the gate still follow the logic table if Vcc was lower than the input?