Other Parts Discussed in Thread: TXB0106
Hi,
We are using TXB0106(TSSOP package TXB0106IPWRQ1 ) for level shfting of signals between FPGA(2.5V) and Audio CODEC(3.3V). We could see level shifting operation happening properly for low frequecies which are around 48KHz. But level shfting is not happening properly for signals of 3MHz frequency. The input to the level shfter is perfect square wave of 3MHz frequency(low level at 0V and high level at 2.5V). At the output of the level shfter we are expecting perfect square wave of 3MHz frequency(low level at 0V and high level at 3.3V). But this is not happening. The output signal frequency is coming 3MHz but it is not square wave. Signal level is slowly rising and slowly falling similar to ramp. The signal swing is between 0.68V and 2.5V against the expected 0V and 3.3V. Due to this issue CODEC is not able to detect the signals properly. We are connecting VCCA to 2.5V with 0.1uF decap and VCCB to 3.3V with 0.1uF decap. We have tried by increasing the FPGA drive current from 12mA to 16mA but still we could not see any improvement. Please help us to resolve this issue.
Regards,
Narayana Rao