This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Add a time delay to signal going high to low

Hello,

I have a CMOS 3.3V output level that goes high when no signal is present. When the signal is present the output low drops low.

I am looking for a way that I can take that signal and add keep it high when it drops low for an adjustable time from approximately 0 seconds to several hundred milliseconds.

I do not want to affect the turn on time of the signal at all.

Is there some IC that will do this using a single resistor for the delay time? I need something as simple as possible.

Best Regards,

Scott