This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CB3T16212ZQLR - Materials Declaration



Hello,

My customer is looking the tin/silver/copper alloy content (in percentages) of the lead free solder balls used in the TI SN74CB3T16212ZQLR. They need to find out the percentages, which usually show up in a Materials Declaration Data Sheet for the package.  They are looking to find out if it is SAC405 (4% silver), SAC305 (3% silver), SAC105 (1% silver) or some other combination of alloys.

Thanks,
Alex

  • Alex,

     Go to the Product Folder page:   http://www.ti.com/product/sn74cb3t16212 .

     scroll down to Quality, for the ZQL package, click on View:

    You'll then see:

    Quality - Eco-Info & Lead-free (Pb-free):Content & Schedule Search Results

    Under the Part Number Details, click on the TI part number, you'll see a full listing of all aspects of the device, including the Solder Ball section:

    http://focus.ti.com/quality/docs/searchbypcid.tsp?templateId=5909&navigationId=11220&PCID=51144&OrderablePart=SN74CB3T16212ZQLR

    Solder Ball
    Aluminum & Its Alloys Aluminum 7429-90-5  0.000155 0.0020 19 0.0003 2
    Copper & Its Alloys Iron 7439-89-6  0.001550 0.0200 199 0.0026 26
    Copper & Its Alloys Zinc 7440-66-6  0.000155 0.0020 19 0.0003 2
    Nickel & Its Alloys Nickel 7440-02-0  0.003875 0.0500 499 0.0065 65
    Other Nonferrous Metals and Alloys Antimony 7440-36-0  0.009300 0.1200 1199 0.0157 157
    Other Nonferrous Metals and Alloys Arsenic 7440-38-2  0.002325 0.0300 299 0.0039 39
    Other Nonferrous Metals and Alloys Bismuth 7440-69-9  0.007750 0.1000 999 0.0131 130
    Other Nonferrous Metals and Alloys Cadmium 7440-43-9  0.000155 0.0020 19 0.0003 2
    Other Nonferrous Metals and Alloys Lead 7439-92-1  0.003875 0.0500 499 0.0065 65
    Other Nonferrous Metals and Alloys Proprietary Metals (including Ag and Cu) 7440-22-4, 7440-50-8  0.131755 1.7000 16999 0.2226 2226
    Other Nonferrous Metals and Alloys Tin 7440-31-5  7.589401 97.9240 979240 12.8239 128239
    Sub-Total   7.750296 100 1000000 13.0958 130953

     

  • FYI, because it wasn't spelled out and the question was asked in this manner,  for the ZQL, the material is SAC125  (Sn/Ag1.2/Cu0.5)