This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0108 for PCI 2.2 level translation

Other Parts Discussed in Thread: TXB0108

For our project we want to connect FPGA Virtex 6 to a legacy PCI plug-in card. Virtex IO supply max is 2.5V and the PCI card operates at 3.3V. For this we wanted to use level translator. The general level translators can not be used since PCI works on reflected-wave switching where the input voltages will be higher than the IO voltage and may damage the level translator. Can we use TXB0108 device for level translation for PCI application? 

Thanks in advance.

Naveen