This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G17 logic buffer: can it drive a long PCB track with 75Ohm impedance parallel terminated by 75Ohm resistor at the end?

Other Parts Discussed in Thread: SN74LVC1G17

Hi:

  I need to select a buffer for a 3.3V logic sigal from CPLD. The signal is a few MHz can have to travel 3 feet long of PCB track.

 If the pcb track impedance is 75Ohm, and I use 75Ohm parallel termination. Then the current consumption is 3.3V/75Ohm=44mA.  But the SN74LVC1G17 output is 24mA.

I can not find another proper logic buffer for this case. Is there a dedicated buffer for driving tranmission line or coaxial cable with parallel termination?

Thank you!