This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NEED INFORMATION- SN74LVC2244APWR and SN74LVC16245ADGGR

Hi Can you please provide the following information for the  SN74LVC2244APWR and SN74LVC16245ADGGR

Part ?

1. Thermal Resistance Junction to Case (Theta JC)

 

Regards,

Jayakumara K

  •  

    Package Die Size
    (mils)
    Pad Size
    (mils)
    Low or
    High K
    Data
    Source
    Tja Pjt Tjc Tjp Tjb Derating
    Curve
    Update
    0 LFM 150 LFM 250 LFM 500 LFM 0 LFM 150 LFM 250 LFM 500 LFM
    14PW 48 x 53 71 x 71 High Model 112.6 105.6 102.3 97.0 2.40 4.00 4.60 5.60 46.6 72.7 Plot Update
    16PW 62 x 62 104 x 104 High Actual 108.4 102.3 99.9 95.9 1.10 2.40 2.90 3.70 33.6 Plot Update
    20PW 53 x 69 102 x 106 High Model 83.0 77.9 75.4 71.4 1.00 2.20 2.60 3.40 32.3 Plot Update
    24PW 62 x 62 94 x 140 High Actual 87.9 82.4 80.4 77.4 0.60 1.70 2.00 2.70 25.7 Plot Update
    28PW 78 x 137 110 x 198 High Model 61.7 55.1 52.7 49.2 16.4 Plot Update
    8PW 62 x 62 67 x 79 High Actual 149.4 142.0 138.2 132.4 7.60 10.00 10.90 12.40 65.1 Plot Update

     

    Package Die Size
    (mils)
    Pad Size
    (mils)
    Low or
    High K
    Data
    Source
    Tja Pjt Tjc Tjp Tjb Derating
    Curve
    Update
    0 LFM 150 LFM 250 LFM 500 LFM 0 LFM 150 LFM 250 LFM 500 LFM
    48DGG 120 x 120 126 x 181 High Actual 70.0 65.3 63.5 60.9 0.00 0.10 0.10 0.20 18.2 32 Plot Update
    56DGG 120 x 120 154 x 201 High Actual 63.8 59.3 57.7 55.2 0.10 0.40 0.60 0.80 14.2 Plot Update
    64DGG 120 x 120 138 x 270 High Actual 55.4 51.1 49.6 47.3 0.21 0.80 1.00 1.35 13.6 Plot Up