This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXB0108 OE question



Hello:

I'm looking to use this part on my design.  It states that OE is referenced to the Vcca which for me is 1.8V.

It looks like this could be tied to 3V though and hoping you can confirm this as well.

http://www.ti.com/lit/ds/symlink/txb0108.pdf

Any feedback or input is welcomed and appreciated!

Thanks again!

Paul

  • Hello Paul,

    OE is supplied by VCCA, which can be 1.2V to 3.6V.
    VIH input high max for OE is 5.5V, min isVCCA x 0.65.
    This is on page 4 of the datasheet.

    Be aware of NOTE (2)

    (2) VCCA must be less than or equal to VCCB and must not exceed 3.6 V.