Other Parts Discussed in Thread: TXB0108, ADS1299
Hello!
I'm using a TXB0108 in conjunction with an ADS1299 and an AVR. The problem that I'm having is that my output voltages for time-varying signals are low or non-existent. The set up is as follows:
Vcca = 3.3V
Vccb = 5V
OE = Vcca = 3.3V
My 5Vpp clock signal just doesn't show up on the corresponding output pin, for instance. It just hovers around 1.5V or so. However, 5V DC will be properly translated down to 3.3V.
I don't think that it's a pull up/down thing on the inputs to the ADS1299. I double checked this by trying with an unused pair of pins and encountered the same problem.
thanks!