Other Parts Discussed in Thread: TXS0108E
Hello, I would like to convert the 1'8V from the I/O expansion port to 3'3V or 5V, so I have been seeking on Internet and I found two options: - TXS0108E: 8-Bit Bidirectional Voltage-Level Translator For Open-Drain And Push-Pull Application.But I have a couple of questions: 1.- For the I2C , SPI and UART should I use the TXS0108E (For Open-Drain And Push-Pull).I want to use this level shifter for UART based GPS and SPI based temparature sensor application. Can any body please suggest me for right selection of level shifter.
Regards,
Sriman.