Hi all,
i need to translate a (0,+15V) analog input to the range accepted by ADS1675REF board.
I've seen that the common mode voltage for this board is 2.5V and the ADS1675 input range is ±Vref so from datasheet i suppose is ±3V.
If i am right all this drives to an input that must lie inside a [2.5-3, 2.5+3] so finally i have to scale (0,+15) to (-0.5V, 5.5V) isn't it?
Any suggestion about circuit to realize this?
Thanks in advance
MR