Hello
I need to be able to select/switch about 20 digital 3.3V signals från two sources into one destination. Some of the signals are inputs and the other are outputs.
Should I select an analog multiplexer or a digital multiplexer/demultiplexer?
The maximum signal frequency is max 50 MHz.