Other Parts Discussed in Thread: TCA9554, PCA9534, PCA9554
Hi!
I am looking into if I should use the PCA9534 or the TCA9554. What is the difference between these devices?
Best regards, Martin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Martin,
From the specs on the product page, it looks like the difference between the PCA and TCA would be the voltage range. The PCA range is 2.3 to 5.5V and the TCA is 1.65 to 5.5.
The difference between the PCA9534 and PCA9554 (TCA9554) is that the PCA9534 is a low power version that does not have an internal I/O pull up resistor.
The fixed address for both devices are the same and allow for up to 8 devices on a single bus. The A version of each allows up to 16 devices on the same bus.
Inside the PCA9534 data sheet you can find a comparison chart for the different devices in the PCA and TCA families.
Thanks,