For this SN74LVC1G07DCKR – Single buffer with open-drain output, what is the Voh (min) and Voh (max) when supply with 3.3V with different output current level?
Output Current, Ioh : 0mA ~ 3.5mA
Voh min : ?? Voh max : ??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
For this SN74LVC1G07DCKR – Single buffer with open-drain output, what is the Voh (min) and Voh (max) when supply with 3.3V with different output current level?
Output Current, Ioh : 0mA ~ 3.5mA
Voh min : ?? Voh max : ??
Hi Lennon
This part has an open drain output and the Voh will be whatever you pull it up to. It will have no high drive and the output can be pulled up to any voltage from 0 to 5.5V