Other Parts Discussed in Thread: AM3715
Hello
I want to use TX0108E devide to translation the 1.8V AM3715 JTAG signal to 3.3V.
In the data sheet it is specify that the maximum continuous current through VCCA, VCCB and GND is 100 mA. On the other hand in the same table it is specify that the maximum continuous output current is 50 mA (I undertand that this value is per pin, am I right?).
Can`t the continuos output current be higher than 100 mA?
Can I used this devide for the application listed aboved?
Best Regards,
Alberto