This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unused switch inputs on TS3DV621RUAR

Datasheet for TS3DV621RUAR does not say anything about unused  switch inputs/outputs. In my application, there will be unused inputs/outputs. All control signals (EN, SEL1, SEL2) will be used. Some of switch inputs/outputs will not be used. Note that I am using word "inputs/outputs" because bidirectional LVDS signals will be switched.

The question is:

Is it OK to leave the following pins on TS3DV621RUAR floating: AUX+A, AUX-A, HPDA, CECA, AUX+B, AUX-B, HPDB, CECB, D3+A, D3-A,  D3+B, D3-B, D3+, D3-, HPD, CEC?

Regards,

Slavisa