This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

One chip interface CMOS logic to 1.2V motor?

Other Parts Discussed in Thread: SN754410

I have searched the TI website for a while now and have not quite found a chip suitable for my application. It seems as though a one- or two-chip solution should exist; I'd like to ask for help in finding it. I have in mind a toy similar to the remote-control "Bitchar-G" miniature cars that were so popular a few years ago. This toy runs a small cell-phone vibrator motor and a small solenoid directly from a 1.2-1.5 volt rechargeable lithium battery. A voltage converter boosts the supply voltage to 3.0 V to run the radio receiver. I would like to use the boosted supply voltage to run an MSP430 device, giving the car a "brain". I would like a chip or FET array that will take CMOS level control signals and switch the direct battery current at the 1.2-1.5 V level to control the motor and solenoids. The SN754410 would look like a good solution, but requires a minimum supply voltage of 4.5 V. Do you have any suggestions? Sincerely, Bryan J. Lowder

Thanks to anybody who can help. -BJL