This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC4060 Doesn't work with a 32.768kHz oscillator?

Other Parts Discussed in Thread: CD74HC4060, SN74HC4060

Hi, the bellow circuit doesn't work. 

VDps=3.6-4.2v

When I use a 4MHz oscillator it works perfectly.

If I use a CD74HC4060 it also works.

Why wouldn't it work with the SN74HC4060?

Michael