Hi TIer
Is it possible to tranmit 110MHZ clock signal with SN74AVC16T245?
Additionally, what is the maximum speed of this device.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TIer
Is it possible to tranmit 110MHZ clock signal with SN74AVC16T245?
Additionally, what is the maximum speed of this device.
Jake,
I would probably not recommend using the SN74AVC16T245 for a signal with a clock of 100MHz.
The recommended operating condition for input transition rise/fall time is 5ns/V.
If the VCCA side is operating at 1.2V, then a single CLK period should take at least 12ns, which correlates to only 83MHz.
There are not many parts that have 16-bits available, but there are many 8-bit translation parts. Would you consider using 2 of these parts as a replacement for the SN74AVC16T245?
What is the application? What is being applied to the A-port? B-Port?
Thanks,
Brian
Thank you for prompt answer.
I need correct that you mentioned before.
Actually Clock frequency is 110MHZ for using PCI-E.
And, You might have a typo on recommendation part that is same part what I ask.
Also I am going to share what you ask as below.
1. Application : Tester for camera module.
2. A side : 1.8V. B side : 3.3V
Hope to see your answer.
Jake,
I think you may have misunderstood:
Dear Brian.
I have same questions.
Plz let us know which devices you recommend to get the higher speed if I use 2 8-bit level translators.
Thanks.
Can you please tell me the VOH and VOL levels for the B-side port?
i.e. what are the voltages for a logic high and logic low that will come from the PCI-e card operating at 3.3V?
As I understand it, PCI-e operates using a low voltage swing to signal high and low logic, referenced at a mid-rail voltage
Our voltage translators may have difficulty translating for PCI-e due to a low voltage signal swing about a mid-rail reference voltage. For example, if the mid-rail is VREF, then Data+ may be only VREF+0.5V and Data- may be only VREF-0.5V which would mean our voltage translators would not see a low-to-high or high-to-low transition.
Thanks,
Brian