This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LV4052A wiring

Am I reading the datasheet correctly in assuming these pin connections:

VCC <-> 3.3V

GND <-> GND

1-COM <-> GND
2-COM <-> GND

2Y0 <-> Audio Source
2Y1 <-> Audio Source 
1Y0 <-> Audio Receiver
1Y1 <-> Audio Receiver

INH <-> GND
B <-> GND
A <-> GND

This will route the audio from 2Y0 to 1Y0, and the max peak to peak voltage that can be switched is 5.5V, with the MIN of the waveform at GND.