This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I2C device



Hi all.

Look for an I2C device immediately.
Before, there is a question about the following
 TI article introduced as a compatible article of the multiplexer.

SN74CBTLV3251PWR
SN74CBTLV3253PWR

Although a Data signal can be used in both directions and is so,
 as long as the data sheet of a headquarters article is seen,
Is use possible also as Multiplexer of I2C (bidirectional signal)?
(Although it thinks that use is possible, it will be saved,
 if the reason is also taught and got when it cannot be used)

Moreover, as a multiplexer for I2C,
if there is a recommendation article of the function independently.

Best Regerds,
Hisa Kobayashi.