Good Day,
We are using the CD40109B in high to low configuration:
VDD=3.3V
VCC=15V
All Enable (2,7,9,15) = 15V
Input threshold is 0.85V (H-L transition) / 1.15V (L-H transition):
This doesn't seem to comply with the datasheet. Can you please investigate?
Best Regards,
Burkhard