In the PDF datasheet there is conflicting data on the temperature range of this device.
On page 2, it shows the device as have Ta of -40C to 85C.
On page 11 (in the addendum), it shows it as -40C to 125C.
Product page calls out 125C, but that might have been dependent upon which number was pulled from where in the datasheet...
At least some distributors are calling out 85C.
And I do note that NXP's version (while it has the same 0.5mm pitch, it does NOT share the same footprint! Very disappointing!) is rated to 125C.