Other Parts Discussed in Thread: CD4010B-MIL, CD4010B-Q1
Hello,
We need a small variety of logic functions that will operate in an -10 to +135 C environment.
Since there does not seem to be anything meeting this rating, I thought of using parts similar to the
CD4010B-Q1 or CD4010B-MIL for example and replacing the unit when it fails.
Do you have any statistics for reliability at the this temperature or maybe any other suggestions?
I should have stated that the application calls for logic that can operate between 2 - 8V within the
above temperature range.
Thanks
David