Hi,
I'm using SN74AVCH4T245PWR IC for a project, and one of the 4 data lines (A1,B1) is to be used for a bi-directional signal between a test chip and an FPGA. VCCA=VCCB=3.3V. I referred to the "SCLA015" app note, and most of my doubts were cleared, but I had a few more queries regarding the bus hold circuitry functioning here,could you please provide some help with them:
1.First let's assume data is transmitted from A1 to B1. I force logic 1 on port A1 first (1DIR being high and 1OEZ being low, ie, output is enabled) and it appears on B1. Now if I make 1OEZ high(thus disabling the outputs), by bus hold operation,will logic 1 still be maintained on bus B1, irrespective of the signal that is applied on A1 and signal on 1DIR as long as 1OEZ remains high(assuming B1 isn't driven from the opposite side)? Basically I'd like to know if the combination of bus hold circuitry and OEZ function used as a sort of latch to latch the last input on A1 on port B1 by making OEZ high.
2.If yes, the logic 1 on bus B1 that is held by bus hold can reliably drive another buffer connected to B1 as long as the buffer draws in less than 100uA?
3.Now if I make 1DIR low(such that data should flow from B to A), and enable the output by making 1OEZ low, now the external driver connected to B1 has to sink at least 500uA, if it were to transmit a logic 0 to port A1 right?
Thanks,
Anoop