This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Best line driver for 75 Ohm cable

Other Parts Discussed in Thread: BUF602, OPA693, LM6171, LM7171, CLC001, SN65ELT20

Hi,

I'm searching for 2 line driver for a single ended connections to a 75 ohm cable. High speed (>100 MHz) and high output current is required (> +/-30mA). I found some options like, 74AS808, 74AS1008, 74ABT125, 74ABT126, 74AS1034A. Is there any other option available/advisable part for this kind of operation? Can I protect the output against short circuits without compromising the speed operation? Thanks!

Regards,

MC