Other Parts Discussed in Thread: SN74LV8153
I'm wondering if I can use the SN74LV8153 to drive a 12V relay. Coil imp is 390 ohms, so IOL required is 31mA. DS says it can handle 40mA but suggests this is only with VCC2 at 4.5V. VCC2 will need to be at 12V. DS not explicitly clear on 12V drive capability.
Thanks,
Mike