I am trying to use the SN65LVDS1DBV to translate a 'clipped sine wave', which is a 0 to 1V psuedo-square-wave to translate to an LVDS input to a DAC Clock. Can I achieve this with this part and how? Do I need to bias the input to the part & at what level. I know the part works with a CMOS level because that is what I have now, but I want to try a new reference clock that only has this lower level output.