Other Parts Discussed in Thread: TXB0101
Hello,
My customer uses TXB0101. He operates it under conditions as follows.
VCCA=1.8V VCCB=3.3V
Connect to external IC by 40ohrm series resistor. Not pulldown or pullup.
So there is a slightly chattering noise in rise edge and fall edge at Vcc1/2.
The noise occur both from A to B and from B to A. It occur only B port.
He worry about the TXB0101 is miss operation by this noise.
I think the noise is occurred due to impedanse change at Vcc1/2.
Does the series resistor have a bad influence?