This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74LVC1G125DBV Operating Temperature Question



I'm planing to use SN74LVC1G125DBV to convert SIO pin (SPI) into MOSI and MISO in a temperature sensor EVM board that could run at 200℃. So the components in this board are required to work at 200℃. 

But I'm not sure if this 3-state buffer could work or not when temperature rises up to 200℃, even though the datasheet shows its operating free air temperature is from -40℃ to 125℃.

If not, is there another 3-state buffer with the same function could work under 200℃? Please recommend it if you kown.

Eric