Other Parts Discussed in Thread: TXS0101
Hello,
I've got an application where on I/O connection of the TXS0101 requires a bootstrap setting of below 0.25V. Taking into account the 10kOhm pull-up internally (to 3v3) in the TXS0101, I have to use a pull-down resistor of approx. 800 Ohm. On the other side of the translator I've got a driver that is capable of sourcing 5mA. Summarized: Vccb = 3v3, I/O B = pulled down with 800Ohm. Vcca = 1.8V, I/O A is driven to 1.8V with a 5mA capable driver.
Is the TXS0101 capable of driving the 800Ohm resistor with enough current to get a voltage level of >2.5V?
Are there some formulas available for calculating min/max pull-up/down values?
Thanks,
Ingmar