This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Ron value for SN74CB3T3257 at Vi greater than 0V



Hi there,

The datasheet specifies the Ron value for 2.3V VCC and 3V VCC with the Vi set to 0V.  It doesn't show what the Ron would be with Vi at various values such as 1.7V or 2.4V.  Unlike the CB3Q which have a pretty flat Ron response, the CB3T is likely to shoot up at higher voltages.

Can you please confirm if there is any characterization data for this?

Thanks