Other Parts Discussed in Thread: TS5A3157
Hi
Can TS5A3157 connect NC to Vcom when Vcc is OFF?
Best Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
This part does not have the Ioff feature so it may leak some when powered off.
This part would not leak when Vcc = 0V TS5A63157
The TS5A3157 doe not have Ioff feature so there could be some leakage from IN to NC when Vcc is 0V
The output NC will not be connected to INso it should be floating if Vcc = 0V.
If Vcc is floating when it is Off then the output will be unknown. The important thing is to be sure Vcc = 0V when off and not floating at some unknown level