This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TXS0108 used in I2C, 1.7V rather than 3.3V when bus is idle

Hi SC colleague,

My customer starnet is using TXS0108 to translate I2C between 2.5V and 3.3V. But they have an issue. with our devices connected, the bus voltage is down to 1.7V at B side(3.3V side). 

They have tested

1 With or withou external pull-up resistor, the problem existed.

2 OE is pulled down, it is 3.3V on the bus. but when oe is pulled up, the 3.3V drops to 1.7V.

 

Do you have the same problems before?

Regards

Michael