This item supplies me with a crucial parameter, very fast rise and fall times, about 2ns worst case. I have an ac signal that MAY be superimposed on a dc level of varying value. I can limit the peak to < Vcc, but the signal may swing into the negative. I am considering using a supply of +/- 1.35V to allow this to happen without damage to the device, but wonder what issues this will create. I do realize that the digital control will need to be referenced to the negative rail. I could run this switch with a positive supply only, and current limit the input, allowing the input signal to go negative without incurring damage, but I also need the ac component of the signal to remain intact, not severely distorted and that I'm not sure about.
Any thoughts?