This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74AHCT574: old design works differently than new design

Guru 20045 points
Other Parts Discussed in Thread: SN74AHCT574, TMS320F28335

Hello,

I previously asked a question about the SN74AHCT574 (http://e2e.ti.com/support/logic/f/151/t/349518.aspx).

We have an old design (5V design) that is as follows:
uP (5V) --> 3 to 8 decoder (Active Low output, 5V) -> CLK (Pin 11 of SN74AHCT574, 5V)
5V --> inverter (5V) --> OE_N (Pin 1 of SN74AHCT574, 5V)

With the old design, all the outputs are low at power-up. Also, the OE_N follow the CLK Input signal (rise at the same time).

We created a new design (3.3V and 5V design) as follows:
uP (GPIO with internal pull-up of TMS320F28335,3.3V) --> Pull-up (3.3V) --> CLK (Pin 11 of SN74AHCT574, 5V)
5V --> inverter (5V) --> OE_N (Pin 1 of SN74AHCT574, 5V)

With the new design, some of the outputs go high temporarily at power-up. Also, the OE_N reaches 2V (Logic high level) several milliseconds before the CLK Input signal.

Oscilloscope outputs for both the new and old design are shown below (yellow trace is OE_N and pink trace is CLK).  

In both designs, the SN74AHCT574 outputs are ONLY connected to the inputs of a ULN2803A.

Is there a way to correct the issue with outputs going high temporarily at power-up?

Another thing that I noticed is in the new design the SN74AHCT574 outputs are approximately 1V after reset (yellow trace is OE_N and pin trace is SN74AHCT574 output).  What could be causing that issue?

Stephen

Old Design:

New Design:

SN74AHCT574 outputs 1V after reset (New Design):