This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Multiplexer or demultiplexer?



Is there possible to find an integrated circuit that can do following: 5V shortly pushed signal on Input0 and permanent switched 5V on Output0 ? If the 5V impulse is pushed on Input1 the Output0 will be released and moved to the Output1. I need 8 Inputs coresponding to 8 Outputs and every one should work separate. As example, with an 8 keys Keyboard. If i touch the no.1 key i need to have 5Volts only on Output0. Touching the key no.2 i need to have 5volts only on Output1 and so on trough Out7. Thank you in advance. With kindly regards.