Other Parts Discussed in Thread: TXS0104E, SN74AVC4T774
Dear Forum,
I have just started testing a cape for the BeagleBone Black. I have equipped the GPIO lines with TXP0104DR level translators. At the test, VCCA=VCCB=3.3V.
Setting the I/O lines as outputs and applying static high/low results in correct 3.3V/0V ouput levels.
However, If I connect one line to the gate of a MOS transistor and a 180K pull-up, odd things happen.
When connecting the I/O line while high, it remains high. But when setting it low it settles on 1.604V and seem to latch up there. Setting the line high again rises the voltage to 1.628V.
The resistive load > 50KOhm and capacitive load <70pF should be OK for the translator.
Please advice (Schematics attached).
Best regards
Terje Froysa