This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS3L110 - 2:1 multiplexers for RMII Interface

Guru 19785 points

Other Parts Discussed in Thread: TS3L500, TS3L301, TS3L110, SN74CB3Q3257

Hi Team,

Our customer is looking for a 2:1 multiplexer which could use in RMII interface.

I believe there are 4 channels for TX and 4 or 5 channels for RX in RMII, so I think 4 or 8 channel type would be good for their application.

[Q1]
Can the following devices be used in the above RMII signal switching application ?

TS3L110, TS3L301, TS3L500

One thing I was wondering is that these devices does not specify Ron at low input voltage such like under 1.0V. This would mean that low Ron is not guaranteed for these devices.

[Q2]
What would be your recommendation for RMII signal switching application ?
Would SN74CB3Q3257 be a better solution for this app ?

Thanks in advance.

Best Regards,
Kawai