This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
My customer would like to use the following input signal.
Can SN74CBT16390 let this input signal go through?
We can’t judge it because input frequency isn’t mentioned in datasheet.
[Input signal]
-Voltage = 1.8V
-frequency = 54MHz Clock
Regards,
Kanemaru
The frequency is no issue but since the CBT16390 is an Nchannel it will have 1V drop at output from VCC.
Vcc will need to be greater than 2.8V.