Other Parts Discussed in Thread: TXS0108E
Team,
Customer wants to use the TXS0108E for an MDIO level shift from 1.2V to 2.5V. They 2.5V side is an unknown connection from an external source and will have a pull-up on that side. What is the lowest value pull-up that we can tolorate? Can a 1ku be used on the 2.5V side?
Also, for example if there is a 1ku pull-up on the 2.5V side do you also need the same value pull-up on the 1.2V side?
Speed is 1Mb's and ideally they would like 4Mb/s but if they need to always be 1Mb/s than that is ok.
Volume is ~ 100ku and this MDIO is becoming a common need we should look into.