Hi,
I'm trying to interface at ATmega328 5v to a Telit GE865 2.8v USART lines using a TXB010x (have tried a 01 and 06 chips). The Tx signal looks very clean however the Rx line is extremely noisy. Has anyone had success with this interface? I've tried pull-up resistors because it looks like the Telit can only supply about 1mA or so while the TXB is looking for around 2mA. Any advice would be greatly appreciated.
Wayne