Hello,
I am considering of using the TXS0102 to perform level shifting for our DDC signals. The DDC signals coming out from our processor is 1.8V and we will need to drive it up to 5V before reaching the HDMI connector. I have few questions and I hope someone can enlighten me.
1) Between the HDMI connector and an external monitor, there is a cable and the cable length is unknown since this depends on the cables the end users use. As a result, we have no idea on the bus capacitance. There is a statement in the spec saying: "Both PCB trace length and connectors add to the capacitance that the TXS0102 output sees, so it is recommended that this lumped-load capacitance be considered to avoid O.S. retriggering, bus contention, output signal oscillations, or other adverse system-level affects". We are worried by the words O.S. retriggering. Do you have a range of bus capacitance that will guarantee the One shot not to retrigger if we keep the bus capacitance within the range? Furthermore, how does the One shot know a retrigger is needed?
2) Could you recommend any voltage translator (1.8V to 5.0V and vice versa) specific for DDC application? Ideally for driving long cable as well.
Thanks